AXIS#.MT.CLEAR

Description

AXIS#.MT.CLEAR clears a motion task from the drive. This command needs one argument in order to clear a motion task. A motion task consists of the following parameters:AXIS#.MT.P, AXIS#.MT.V, AXIS#.MT.CNTL, AXIS#.MT.ACC, AXIS#.MT.DEC, AXIS#.MT.MTNEXT, AXIS#.MT.TNEXT

Example

Clears motion task number 5:

-->AXIS1.MT.CLEAR 5

After performing this command the drive displays the following:

5   0.000 Counts   0.000 rpm   0   0.000 rpm/s   0.000 rpm/s   0   0   0 ms

A value of 0 for velocity, acceleration, or deceleration displays motion task as uninitialized.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command Array

Units

N/A

Range

0 to 31

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.CLEAR 0

50d1h

01h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 1

50d1h

02h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 2

50d1h

03h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 3

50d1h

04h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 4

50d1h

05h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 5

50d1h

06h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 6

50d1h

07h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 7

50d1h

08h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 8

50d1h

09h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 9

50d1h

0ah

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 10

50d1h

0bh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 11

50d1h

0ch

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 12

50d1h

0dh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 13

50d1h

0eh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 14

50d1h

0fh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 15

50d1h

10h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 16

50d1h

11h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 17

50d1h

12h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 18

50d1h

13h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 19

50d1h

14h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 20

50d1h

15h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 21

50d1h

16h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 22

50d1h

17h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 23

50d1h

18h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 24

50d1h

19h

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 25

50d1h

1ah

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 26

50d1h

1bh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 27

50d1h

1ch

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 28

50d1h

1dh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 29

50d1h

1eh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 30

50d1h

1fh

Unsigned32

-

-

Write only

No

AXIS1.MT.CLEAR 31

50d1h

20h

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6301

1

6301 (0x189d)

AXIS1.MT.CLEAR

Unsigned8[32]

Read/Write

No

71837

2

6301 (0x189d)

AXIS2.MT.CLEAR

Unsigned8[32]

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.CLEAR

6301

Unsigned8[32]

Read/Write

-

Related Topics

Motion Tasks